Merek kami

Selamat datang di Situs Web Schneider Electric

Selamat datang di situs web kami.
		
Bagaimana kami dapat membantu Anda hari ini?
How can I get a demo of OFS
Issue
How to get a demo of OFS

Product Line
OFS

Environment
Windows 10

Resolution
Use the following steps to download a copy of the latest version of the OFS installation CD to get the demo.  To get the latest
updated demo version, download the latest service pack.

Navigate to 'https://www.se.com/ww/en/download/'
  • Type in OFS within the search window.
  • Click on search.
  • Select the latest version or service pack.
  • Download the file
  • Extract the contents of the zip file to a temporary folder.
  • Run Setup.exe.
  • Use the part number TLXCDLTOFS36
  • Use the serial number 99999999999

This will provide a 2 hour demo for 21 days.