FAQ Pencarian
How to activate the Site Manager with Vijeo Designer runtime
The HMI RunTime includes the SiteManager software if the hardware target supports it.
To activate this feature in Vijeo Designer target:
Enter offline mode, click "Main Unit Settings / Remote Viewer Settings", then select "SiteManager Embedded".
To activate this feature in Vijeo Designer target:
Enter offline mode, click "Main Unit Settings / Remote Viewer Settings", then select "SiteManager Embedded".
- In order to start the SiteManager software, set "Remote Management"/"Access Control" to "Enable"
- In order to stop the SiteManager software, set "Remote Management"/"Access Control" to "Disable"
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: