Merek kami

Selamat datang di Situs Web Schneider Electric

Selamat datang di situs web kami.
		
Bagaimana kami dapat membantu Anda hari ini?
Can I change the date/time in an ATV340 series drive via SoMove or the Web Server?
Issue:
Is it possible to modify the date/time information in the ATV340 drive through SoMove/Web Server?

Product Line:
ATV340 series drives.

Environment:
All models and serial number as of 10/22/18

Cause:
Clarification of characteristics

Resolution:
It is not possible to modify the date / time of the ATV340 series via SoMove. Currently, it is not possible to update the date/time of the ATV340 series via the web server. This is a known issue with original drive, however, should be corrected in a firmware updates after in Q1 2019.

Currently, to set the date/time in an ATV340 series drive, enable the SNTP server so allow the drive to pull the date/time from the network clock.