FAQ Pencarian
What can cause a CFI2 [Conf Transfer Error] on an ATV340 series drive?
Issue:
Customer is experiencing a CFI2 fault on an ATV340 series drive.
Product Line:
ATV340
Environment:
Not applicable.
Cause:
Resolution:
Customer is experiencing a CFI2 fault on an ATV340 series drive.
Product Line:
ATV340
Environment:
Not applicable.
Cause:
The configuration has not been transferred properly.
The configuration loaded is not compatible with the drive
Resolution:
Check the configuration loaded previously.
Load a compatible configuration.
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: