Pump runtime can be reset by writing zero or can be set to a value written over communication. Pump runtime cannot be reset via SOmove or HMI.
See attached list of addresses for each pump. Writing is possible when the drive is stopped (not in run state). For writing value via modbus or modbus TCP, use logic address. Depending on PLC type you may need to write value to address+1.
Bear in mind that runtime is 32bit value.
For writing the value it is possible to use a free tool like modscan and write value directly from PC
See attached list of addresses for each pump. Writing is possible when the drive is stopped (not in run state). For writing value via modbus or modbus TCP, use logic address. Depending on PLC type you may need to write value to address+1.
Bear in mind that runtime is 32bit value.
For writing the value it is possible to use a free tool like modscan and write value directly from PC
Diterbitkan untuk: Schneider Electric Indonesia


Perlu bantuan?
Pemilih produk
Temukan produk dan aksesoris yang tepat untuk aplikasi Anda secara cepat dan mudah.
Dapatkan Penawaran Harga
Silakan kirimkan pertanyaan terkait penjualan secara online dan pakar kami akan menghubungi Anda.
Tempat pembelian
Temukan distributor Schneider Electric terdekat di lokasi Anda dengan mudah.
Pusat Bantuan
Temukan sumber daya dukungan untuk seluruh kebutuhan Anda, di satu tempat.