FAQ Pencarian
What to do if a message with ID 0x1440, 0x1441 or 0x1442 is displayed on the MicroLogic X screen.
These messages are generated by the Contact Wear Monitoring function of the MicroLogic X control unit, to indicate that a predefined wear threshold is reached.
Refer to the MicroLogic X User Guide:
Refer to the MicroLogic X User Guide:
- For information about the Contact Wear Monitoring function and recommended actions.
- For information about how to acknowledge a message on the MicroLogic X screen
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: