FAQ Pencarian
Are the 8911DPS starters provided with a NO holding contact?
Issue:
Do the 8911DPS starters come with a normally open holding circuit?
Product line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Class 8911 Type DPS NEMA Definite Purpose Starters
Cause:
Customer control wiring
Resolution:
No, the Class 8911DPS starters do not come with any auxiliary contacts as standard. These can be ordered with auxiliary contacts from the factory, or some can be field installed.
Do the 8911DPS starters come with a normally open holding circuit?
Product line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Class 8911 Type DPS NEMA Definite Purpose Starters
Cause:
Customer control wiring
Resolution:
No, the Class 8911DPS starters do not come with any auxiliary contacts as standard. These can be ordered with auxiliary contacts from the factory, or some can be field installed.