FAQ Pencarian
Is it possible to connect PowerTag C devices (I/O and 2DI) to SmartLink SI B or SI D ?
PowerTag C A9XMC1D3 and A9XMC2D3 cannot be connected to a Smartlink A9XMZA08 or A9XMWA20.
PowerTag C devices are only compatible with PowerTag Link gateways A9XMWD20 or A9XMWD100 with FW 1.4.5.
PowerTag C devices are only compatible with PowerTag Link gateways A9XMWD20 or A9XMWD100 with FW 1.4.5.
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: