FAQ Pencarian
What function codes are supported by the I/O scanner for the M340 NOE Module?
Issue:
Supported function codes by the I/O scanner for the M340 NOE module
Product Line:
M340, BMXNOE0110, BMXNOE0100
Resolution:
The I/O scanner for the M340 NOE modules supports Function Codes 3,16 and 23
Supported function codes by the I/O scanner for the M340 NOE module
Product Line:
M340, BMXNOE0110, BMXNOE0100
Resolution:
The I/O scanner for the M340 NOE modules supports Function Codes 3,16 and 23
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Produk:
Jelajahi lebih lanjut
Produk: