Bagaimana kami dapat membantu Anda hari ini?

Which devices need to be installed externally on the EVlink Home charger?

The EVlink Home charger must be protected at least by an overcurrent circuit breaker plus a minimum 30mA earth leakage Type A protection according to IEC 62851-1 and IEC 60364-7-722
Depending on your product, Mx or MNx auxiliary protection is also mandatory in some countries (refer to the user manuel included in the packaging).

Schneider Electric Indonesia

Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: