FAQ Pencarian
Where to find the "Runtime Address" when doing tag integration with Machine SCADA Expert and Machine Expert?
1.Issue:
Where to find the "Runtime Address" when doing tag integration with Machine SCADA Expert and Machine Expert?
2. Product Line:
EcoStruxure Machine SCADA Expert, Harmony P6 ,Harmony iPC ,Box iPC ,Harmony GTU Open Box ,EcoStruxure Machine Expert ,M241 ,M262 ,M251
3. Resolution:
Instead of declaring each variable individually in a driver sheet in Machine SCADA Expert, the Tag Integration tool can be used to attach all the variables from a Machine Expert project to a Machine SCADA Expert project. When configuring the tool, the Runtime Address will be required, in this field the Nodename declared in the My Controller window in Machine Expert can be used, or the Node Address can also be used.
The Node Address can be found by hovering the mouse over the PLC displayed in the My Controller window, it will be located next to [Address].