FAQ Pencarian
Machine Expert and M controllers: How to check for forced IOs in the application code?
The following function which is generic for all M controllers will return True in case of forced IOs:
![Workaround](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0158V00000D3AsqQAF&oid=00DA0000000abSmMAI)
The system library CmpApp needs to be added to the Library Manager.
NOTE: This function works for Embedded IOs, TM3 IO modules and TM3 Bus Couplers.
The system library CmpApp needs to be added to the Library Manager.
NOTE: This function works for Embedded IOs, TM3 IO modules and TM3 Bus Couplers.
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Rentang:
Jelajahi lebih lanjut
Rentang: