FAQ Pencarian
Policy with regards to using APC by Schneider Electric UPS on Life Support Products
Issue:
Policy with regards to using APC by Schneider Electric UPS on Life Support Products
Product:
Single Phase Back-UPS, Smart-UPS
Environment:
Global information about APC UPS units
Recommendation/Solution:
APC will not knowingly sell its products for use in such applications unless it receives in writing assurances satisfactory to APC that:
- the risks of injury or damage have been minimized
- the customer assumes all such risks, and;
- the liability of American Power Conversion is adequately protected under the circumstances.
Examples of devices considered to be life support devices are
- neonatal oxygen analyzers
- nerve stimulators (whether used for anesthesia, pain relief, or other purposes)
- autotransfusion devices
- blood pumps
- defibrillators
- arrhythmia detectors and alarms
- pacemakers
- hemodialysis systems
- peritoneal dialysis systems
- neonatal ventilator incubators
- ventilators for both adults and infants
- anesthesia ventilators
- infusion pumps, and;
- any other device designated as critical by the U.S.F.D.A.
NOTE : Hospital grade wiring devices and reduced leakage currents that meet medical safety standards may be ordered as options on many APC UPS systems. APC does not claim that units with these modifications are certified or listed as such by APC or any other organization, therefore these units do not meet the requirements for use in direct patient care.
Diterbitkan untuk:Schneider Electric Indonesia
Jelajahi lebih lanjut
Kategori:
Rentang:
Jelajahi lebih lanjut
Kategori:
Rentang: