FAQ Pencarian
PME2023 - Error occurred when import "PME - Binding Template.xml" in PME 2023 ISO
Important Update: New PME Binding Templates Available
Issue:
The PME binding templates.xml included in PME2023 ISO is outdated.
In the "..\EBO Integration Files\WorkStation" folder. This file "PME - Binding Template.xml" is made as an export for SBO version 1.5, which is not compatible with the latest EBO. Therefore the import will fail with error
How to Access the New Templates:
Customers can access the updated PME - Binding Template v5.0.2.xml by downloading the attachments provided in this FAQ.
Important Note: It is important to note that the PME binding templates provided in PME 2023 ISO are no longer recommended for use. Customers are advised to transition to the updated templates to benefit from the improvements and optimizations.