FAQ Pencarian
BACnet map for Single Phase UPS units with APC Network Cards
Issue:
Looking for the BACnet map of Single Phase UPS units with APC Network Cards
Product:
APC single phase UPS (SMT, SMX, SMTL, SRTL, SURT, SURTD) units global offer with APC Network Management Cards (BACnet capable)
Environment:
APC single phase UPS units global offer with APC Network Management Cards using BACnet applications
Solution:
BACnet is a communication protocol for Building Automation and Control (BAC) networks that use the ASHRAE, ANSI, and ISO 16484-5 protocol standards.
BACnet was designed to allow communication of building automation and control systems for applications such as heating, ventilating, and air-conditioning control (HVAC), lighting control, access control, and fire detection systems and their associated equipment. The BACnet protocol provides mechanisms for computerized building automation devices to exchange information, regardless of the particular building service they perform.
Attached are the BACnet register maps as of the date of this article that are used by our Single Phase UPS units with BACnet capable Network Management Cards.
NOTE : Please always check SE.COM under documents for the latest APC BACnet register maps available