Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Schneider Electric launches the new enhanced GenieEvo with an increased fault rating of 31.5kA

London, UK

08/04/2025

  • GenieEvo 31.5kA offers increased safety and reliability with higher fault current protection 

  • SF6-free intelligent equipment monitoring enables condition-based and predictive maintenance  

Schneider Electric, the leader in the digital transformation of energy management and automation, announces the launch of GenieEvo 31.5kA in the UK and Ireland. 

GenieEvo is an air insulated medium voltage switchgear offering, with safety and reliability at its core. 

Its higher fault current protection of 31.5kA, up from 25kA in previous iterations, enhances safety and reliability. It improves system resilience and reduces the risk of equipment damage in the event of power overloads or short circuits. 

GenieEvo is digital in design and comes with Schneider Electric’s EcoCare membership services plan. It incorporates smart Internet of Things (IoT) sensors which transmit data, in real-time, to experts at Schneider Electric’s Connected Services Hub for monitoring and analysis. This enables condition-based monitoring and predictive maintenance which can cut the number of unplanned outages and ensure a more efficient approach to maintaining equipment. 

It is particularly suited to those with heavy-duty electrical distribution needs such as Distribution Network Operators (DNOs), data centres, and medium to large sites with significant energy requirements. These include industries such as oil and gas, mining, and manufacturing as well as large buildings including airports and hospitals. 

GenieEvo key features include: 

  • A pure air design vacuum switchgear with a high fault current rating of 31.5kA for enhanced safety and reliability  

  • Newly designed C-type bushings which are easy to install offering improved insulation, durability, and thermal management 

  • Innovative 2000A Busbar CTs ensuring high accuracy in metering and monitoring 

  • A-FL switchgear front and side protection for users for Internal Arc Compliance (IAC) 

  • IoT sensors monitoring thermal, environmental, and partial discharge data, 24/7, enabling condition-based and predictive maintenance 

  • A compact design which can reduce space requirements by up to 40%. It comes with pre-engineered panels to meet individual requirements and can scale to meet future needs 

“To enable the energy transition, we need to integrate more energy sources to the distribution network, and this creates challenges, particularly for those with significant electricity demands,” said David Hall, Schneider Electric’s Vice President of Power Systems UK&I. “Organisations need to take control when it comes to safety and reliability and should look at their switchgear as a priority. GenieEvo has been developed in response to market demands allowing them to do just this.” 

Schneider Electric will manufacture the GenieEvo at its Leeds site, which had a £7.2million investment in 2023 to meet the increasing demand for Schneider Electric’s portfolio of switchgear products.  

Related resources 

  • Find out more about Schneider Electric’s GenieEvo offering 

  • Video and eBrochure 

 

About Schneider Electric  

Schneider’s purpose is to create Impact by empowering all to make the most of our energy and resources, bridging progress and sustainability for all. At Schneider, we call this Life Is On. 

Our mission is to be the trusted partner in Sustainability and Efficiency. 

We are a global industrial technology leader bringing world-leading expertise in electrification, automation and digitalization to smart industries, resilient infrastructure, future-proof data centers, intelligent buildings, and intuitive homes. Anchored by our deep domain expertise, we provide integrated end-to-end lifecycle AI enabled Industrial IoT solutions with connected products, automation, software and services, delivering digital twins to enable profitable growth for our customers. 

We are a people company with an ecosystem of 150,000 colleagues and more than a million partners operating in over 100 countries to ensure proximity to our customers and stakeholders. We embrace diversity and inclusion in everything we do, guided by our meaningful purpose of a sustainable future for all.  

www.se.com   

Hashtags: #PressRelease #PowerSystems #GenieEvo #Innovation #SF6Free #News 

Adoption of Wiztrust's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page: