Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to download Vijeo Designer v6.1 (installer)
In this FAQ you can find attached the installer for Vijeo Designer v6.1.
The software is divided in three (3) parts: Vijeo Designer V6.1.zip.001 , Vijeo Designer V6.1.zip.002, Vijeo Designer V6.1.zip.003 .
Once we download the three (3) we will ned to unzip one of the files to generate the folder with the installer of Vijeo Designer v6.1.

Vijeo Designer v6.1 is not a free software we strongly recommend to work with the latest version of the software Vijeo Designer v6.2 and their Service Pack.

We can not have in the same laptop/computer the software Vijeo Designer v6.1 and Vijeo Designer v6.2.

If we have Vijeo Designer v6.1 licensed we can upgrade it to Vijeo Designer v6.2 but we need to buy the license with the part number VJDUPDTGAV62M.

Schneider Electric Ireland

Attachment(s)
Vijeo Designer V6.1.zip.003 [602.05 MB]
Vijeo Designer V6.1.zip.001 [1000 MB]
Vijeo Designer V6.1.zip.002 [1000 MB]