Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which is the alternative cable for the Unitelway TSXCSA100 / TSXCSA200 / TSXCSA500 ?

Please note that part references TSXCSA100 / TSXCSA200 / TSXCSA500 are discontinued with no direct replacement.

The specifications for the TSXCSA cable are:

•Double twisted pair 24awg

•85 ohm/km

•Shield 12 ohm/km

•Cap 100pf/meter

•Impedance 85ohms

•Attenuation 13 DB/km 0 to 20 KHz

•Max bus 1 km

•PE jacket 9.65 mm diameter

•Belden equivalent 9842

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: