המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
PowerChute Business Edition does not install successfully on Red Hat Enterprise Linux 7.x and Oracle Linux 7.x
Issue:
PowerChute Business Edition (PowerChute) does not install, and the following error message is displayed:
./config.sh:line 130: /bin/java/jre/<jre version>/bin/java: Not a directory

Product Line:
PowerChute Business Edition

Environment:
OS: Red Hat Enterprise Linux (RHEL) 7.x x64, and Oracle Linux 7.x x64
Build: PowerChute Business Edition 9.1.0, 9.1.1, 9.2, 9.0.1, 9.0.2, 9.0.3 OEM Basic and 25 Node Deluxe

Cause:
OpenJDK is installed in the directory used by PowerChute for the bundled private Java Runtime Environment (JRE).

Resolution:
This issue has been resolved in PowerChute Business Edition 10.5

NOTE: PowerChute Business Edition has been replaced with PowerChute Serial Shutdown as of March 2023.
PowerChute Business Edition will be discontinued on April 29, 2024, and support will end on June 5, 2024.