המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can an ATS22 be mounted horizontally?
Issue:
Considering installing an ATS22 by mounting it horizontally.

Product Line:
ATS22

Environment:
All models and serial numbers

Cause:
N/A

Resolution:
The ATS22 is designed to be mounted vertically to provide proper cooling airflow through it.  Mounting it horizontally can lead to excessive heat build up inside the unit, causing premature failures.  As stated in the installation manual, install the ATS22 vertically within +/-10degrees.  Any damage or failure caused by mounting outside of the specification will void warranty.