Issue:
Added security is required.
Product Line:
NetShelter
Environment:
AR8132A
Cause:
It nmay be required to have the combination handles keyed differently.
Resolution:
Yes, the AR8132A can be keyed differently. The lock cylinder is user replaceable.
Please see FAQ FA158606 for additional information.
Added security is required.
Product Line:
NetShelter
Environment:
AR8132A
Cause:
It nmay be required to have the combination handles keyed differently.
Resolution:
Yes, the AR8132A can be keyed differently. The lock cylinder is user replaceable.
Please see FAQ FA158606 for additional information.
פורסם עבור: שניידר אלקטריק ישראל