המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the AQ1 max percent value on the ATV630 and ATV930 process drives when you are outputting mA's for motor current?
Issue:
AQ1 max percent value on the ATV630 and ATV930 when outputting mA's for motor current

Product Line:
Altivar ATV630 and ATV930 drive

Environment:
All

Cause:
100% means 2X the drives current IN ratings.

Resolution:
[Motor Current] OCr Current in the motor, from 0 to 2 In (In = rated drive current indicated in the
Installation manual and on the drive nameplate)

If you want to reduce the range down to 0 to 1 In just change the max percent down to 50%