המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to enable Product Restart via communication for Altivar ATV variable speed drives
There are 2 parameters for product restart.
One is RP. If value 1 is written to RP, the product will restart. In this way product restart can be activated via HMI as well. RP has logic address 16#1BD8 = 7128
Second method is to assign a logic input or a bit written via communication. Assignment can be done via HMI. Somove or communication. See attached table with the possible RPA assignment.
For example if you assign RPA= CD11, the product restart can be activated by bit 11 in CMD word sent by active control channel.

שניידר אלקטריק ישראל

קבצים מצורפים
RP, RPA.txt [4.01 KB]