Issue:
Customer is getting a E18 fault on his ATV212 drive
Product Line:
ATV212
Environment:
E18
Cause:
n/a
Resolution:
E18 fault is a loss of the VIA analog input signal, below the level that is set by Parameter F633. F633 can be set to 0 (disabled) or 1-100 (Fault detection Level).
פורסם עבור: שניידר אלקטריק ישראל