Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do we have MCCB in our range for 400 Hz application.
We have Compact NSX MCCB in our range that can be used for 400 Hz application with a max. breaking capacity “Icu” of 10 kA.
Due to the higher frequency, circuit breakers are subjected to additional temperature rise for identical current levels, resulting from
higher losses caused by Foucault currents and an increase in the skin effect (reduction in the useful CSA of conductors).
To remain within the rated temperature-rise limits of devices, current derating is required.The power levels of 400 Hz applications
rarely exceed a few hundred kW with relatively low short-circuit currents, generally not exceeding four times the rated current.
Please find the below chart for the derating factor for Thermal & Magnetic trip units.

Schneider Electric India

Attachment(s)
MCCB 400Hz.jfif [43.08 KB]
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings