This function is used to force the speed enable in case of emergency
(Fire, smoke extraction …) and NOT stop the drive and motor.
Refer to attached file for more detail of forced & fire functions.
Released for: Schneider Electric India


Our Brands
Welcome to the Schneider Electric Website
Discuss this topic with experts