The Ti24 interface allows direct connection of the Reflex iC60 with 24 Vdc input/output interfaces, e.g. a programmable logic controller.
The Ti24 interface is a 24 V input/output interface.
The Ti24 interface is a 24 V input/output interface.
Released for: Schneider Electric India