The equation for max field resistance = (loop power supply voltage - min ACO output voltage(6V) ) / max output current (25mA).
Example with 24VDC: (24-6)/25 = 720 Ohms
Released for: Schneider Electric India


Our Brands
Welcome to the Schneider Electric Website
Discuss this topic with experts