The limit on the left or the right port for TeSys T Modbus product is the same.
These features are defined by Modbus standard: Maximum 1000 meters without repeater and 31 maximum slaves.
Released for: Schneider Electric India


Our Brands
Welcome to the Schneider Electric Website
Discuss this topic with experts