Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the causes of a CB Control Fault in Sepam relay.
The causes of a CB Control fault are as follows:
1. Circuit Breaker control is turned on and inputs I11 and I12 are not wired.
2. Circuit Breaker control is turned on and inputs I11 and I12 are wired incorrectly. I11 should be wired to the open
status on the breaker while I12 is wired to the closed status.
3. Circuit Breaker control is turned off but inputs I11 and I12 are still assigned to the open and closed status on the
breaker. Reassign to the correct application or other use if not in use.
Note: If SEPAM 80 Series is being used I11 = I101 and I12 = I102.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings