Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the error 8130h means in Advantys Island which consist STB NIP2311 and some digital Input and Output modules.
The error 8130h on an Advantys island generally comes when there is Loss of fieldbus communication, NIM
communication error or internal bus error.
To resolve the problem you can do the following:
1. Make sure that Holdup time in island communication under NIP2311 Module Ethernet Parameter->Master IP, is
greater than the time between two consecutive requests from master. If is not define or varying time to time then put the
Holdup time as 0 will define the infinite holdup time.
The Holdup Time is the amount of time in ms that output modules will hold their current state without any update by
a Modbus write command from Modbus Master. When the module hold-up time out expires, the outputs will be driven
to their defined fallback states.
2. Make sure that the physical installation of the island is correct and all the module and their backplane is properly
installed. Also make it very sure that you have correctly placed the termination module at the end of the island bus.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings