Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can we enable upload the SoMachine application from M258 PLC.
To have the upload feature in M258, the source application or source code need to be downloaded at the time of project
downloaded into the PLC. Without source application inside the PLC it is not possible to upload the application from
M258/LMC058 PLC.
Procedure to download Source Project:
·         Connect to the controller
·         Download the latest version of the application to the project
·         Stop the Controller
·         While Login and the controller stop, download the source project
·         Start the Controller
Procedure to upload the Source Project:
·         Create a new test project with the same M238/M258 model
·         Connect to the controller with downloading any changes
·         Stop the controller
·         While Login and the controller stop, upload the source project

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings