Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the meaning of 1:100 speed range in Altivar 71 drive.
Speed range is the ratio of the output maximum frequency/minimum frequency where the nominal torque is available.
Example: For a 50Hz motor
Altivar 71 in open loop mode, speed range is to 1...100Hz with a nominal speed motor of 50 Hz.
1- 50/100=0.5 Hz and 50/1= 50 Hz
2- The torque curve is guaranty in the speed range of 0.5 Hz to 50 Hz

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings