If drive is Lexium 32C** range, it could be possible via HMI display of LXM32. For this, go to the
CONF menu ==> ACG menu ==> ,nN0 parameter. Actually this is parameter called "InvertDirOfMove"
which is at 0 at default means "Inversion OFF" . If this parameter is changed to 1 means "inversion ON" then
direction of motor movement will be inverted.
For LXM32C range of servo drives parameter ""InvertDirOfMove" can also be modified via modbus communication
at its register address 1560
If drive is of LXM32A** range or LXM32M** range then this parameter has to be modified via SoMoveLite or
Lexium CT configuration software as below.
Released for: Schneider Electric India