Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to control an Altivar 71 from the Keypad.
To control an ATV71 from the Keypad, we have to set Ref.1 Channel [Fr1] in the command menu [CtL] to HMI [LCC].
It is also possible to assign F1.. F4 Keypad Key to [T/K] terminal/keypad.
Once assigned, pressing this key will make the command from keypad.
Refer to attached file for the Fr1 and F1..F4 key assignment parameter.

Schneider Electric India

Attachment(s)
Fr1 and F1 key assignment.pdf [307.53 KB]
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings