Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the usage of DPC function on Sepam series 80 relays? Is it correct if terminal 19-20 bridge from factory ?
DPC is "detection of plugged connectors" bridge on terminals 19-20 of the 20-pin connector which is to be checked and is a mandatory requirement during commissioning. Refer to the attachment for more details.

This will gives the Indication on the display unit that one or more connectors are not plugged in (the detector itself must be connected: see connection schemes). You have to be instal this jumper manually.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings