Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is EPHO fault on Altivar 212 drive.
EPHO is output phase loss fault.
Make sure that there is no output disconnects or output contactor is open before running /stopping.
Example: EPHO comes when we are dropping the output contactor and  when we remove the run command (Give the Stop command). The drive is still trying to ramp down the motor
when the output contactor is being opened. If this is the case, then please do not open the output contactor until the Variable Frequency Drives has ramped down.
It is possible to disable the EPHO fault ,for this, Program the parameter F605 - 0.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings