Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Modicon Quantum comply to IEC61000-4-3 standard
Yes, Modicon Quantum confirms to IEC61000-4-3 standard, IEC61000-4-3 which specify the test method is the "sub-standard" including in IEC61131-2. Schneider has the statement to comply with IEC61131-2.
Inside the official IEC61131-2 document, it mentions the test method confirming to IEC61000-4-3.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings