140 NOC78100 has four ports out of which two ports are meant for control network. These two ports can be configured with Scada for 1gbps connection.
A Control Network is a Ethernet-based network containing PLCs, SCADA systems, an NTP server, PCs, AMS, switches, etc. Two kinds of topologies are supported:
- flat — Devices in this network belong to the same subnet.
- 2 levels — The network is split into an operation network and an inter-controller network. These 2 networks can be physically independent, but are generally linked by a routing device.
Released for: Schneider Electric India