Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to remove or disable the M340 CPU SD memory card
To disable or remove M340 cpu SD card follow the below procedure :-

1. Connect to M340 and make sure the Unity project is Equal, Run and Built.
2. Stop the PLC.
3. Open SD card door.
4. Open the Animation Table Window.
5. Add system bit %S65.
6. Turn on the Modification button.
7. Enter value 1 for %S65. (LED above the SD card will go OUT.
8. Remove the SD card.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings