The maximum allowable distance from ATV71 Drive to braking resistor is 50 meter.
Need to take care about the cross section of the cable to have a low resistance value.
Also it is advise to use a shielded cable with 2 wire for assure the rule of EMC.
Released for: Schneider Electric India