Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to change the IP address of equipment of Harmony HMI runtime using script

You can use set property method for changing the IP address of Ethernet Equipment keeping the parameter for this property as "CON_IPAddress". The methods to be used as follows:

int[] ipAddress = {192, 168, 1, 10};
ModbusEquipment01.openConfig();
ModbusEquipment01.setProperty("Con_IPAddress", ipAddress);
ModbusEquipment01.commitConfig();

Please take note that this is not limited to only Modbus TCP equipments but it can be used for all the Ethernet type Equipments.

Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings