We can set the battery type using the display .
Kindly follow the below mentioned steps to set the battery type
1. Press the ENTER button.
2. Press the UP/DOWN ARROW buttons to navigate to “SET”.
3. Press the ENTER button.
4. Navigate through the parameter (Battery type) using the UP/DOWN ARROW buttons. 'BAT' icon appears on left hand side of display.
5. Press the ENTER button to edit a parameter(Battery Type) > BAT(SF - SMF / VRLA)or (Fld - Flooded / Tubular / Vented). Icons start flashing to indicate the editing.
6. Press the UP/DOWN ARROW buttons to navigate between the options available for the selected parameter(Battery Type).
7. Press the ENTER button to select the option or MUTE/ESC button to abort the editing of current parameter. Flashing of icons stops after this.
8. Press the UP/DOWN ARROW buttons to navigate between parameters.
9. Press the MUTE/ESC button to exit menu navigation.
Released for: Schneider Electric India