The maximum length of the control wires for inputs Y1 and Y2 at a voltage of 230 Vac is:
- 100 metres if a cable is used;
- 500 metres if wires in an electrical duct are used.
The maximum length of the control wires for the Y3 input at a voltage of 230 V DC/AC is 500 m.
- 100 metres if a cable is used;
- 500 metres if wires in an electrical duct are used.
The maximum length of the control wires for the Y3 input at a voltage of 230 V DC/AC is 500 m.
Released for: Schneider Electric India