Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the syntax of the IP address in a READ_VAR or WRITE_VAR block in Unity Pro with an M340?

The syntax for indicating the IP address of the Modbus TCP/IP device to which the READ_VAR or WRITE_VAR function is to communicate is as follows: ADDM('network_link{HOST_ADDRESS.EN_US}') Example: ADDM('Ethernet_1{192.100.200.120}') Illustration:


Description

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings