Motor chokes allow operation with motor cables which are longer than the standard lengths and/or limit the dv/dt at the motor terminals to:
- 500 V/us for 200…400 V and 380…480 V three-phase line supplies
- 1000 V/us for 500…690 V three-phase line supplies
- Limit overvoltages at the motor terminals
- Filter interference caused by opening of a contactor placed between the filter and the motor
- Reduce the motor earth leakage current
Released for: Schneider Electric India