Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Less Back Up issue in BR1500G-IN
1 Check the remaining runtime, load bar graph, percentage of load connected on UPS through the display.
2 How often the power fails(Communicate on the charging period required) Battery needs charging time and communicate the charging procedure
3 What is the Turn OFF procedure at the end of the day(This procedure would  keeps the charger ON and Keeps the battery in charged condition)
Leave the input to the UPS  ON and turn OFF the UPS using the front Panel(You have to follow this process since there is a frequent outage during daytime) this will give an opportunity for the batteries to get charged during night time)
4 How old is the UPS, how many times  do you  face frequent power cuts in a day (Compute the Number of cycles the battery can support)
The batteries could have gone bad, because of the frequent outage, (compute the number of cycles >300 RMA the unit if it is under warranty)
5 Do you have generator installed.
6 Charge the Battery for 72 Hours when runtime is depleting
7  When outage is frequent recommend the customer to shutdown the system immediately

Schneider Electric India
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
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings