Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Getting Message "OLN-11575" in concept V2.6 SR7 while connecting to Controller over Modbus Plus.
Causes:
1. This error comes if you have not set the correct interrupt in the modicon.ini file for modbus plus.
2. Modbus plus card is not available or its driver is not installed.
3. Improper cable connectivity.

Solutions:
1. This error message means that the software interrupt used by the Modbus Plus drivers must be specified in the Modicon.ini file.
For example,
[ports]
MBP0=5C

2. Check for the modbus plus card or converter in programming PC and also check if the relevant driver is installed.
3. Check for the proper cable connection.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings