Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can we use 2 Flying shear blocks in single LMC058 controller.
Yes you can use two flying shear on the same controller. LMC058 controller can handle 8 synchronous axis simultaneously.

But you need to take care that if you want to sync two slave from one master then you must configure two logical axis for master axis and then Link individual Logical axis for each Flying Sheer FB. The reason behind this is using AFB's such as Flying Shear or Rotary Knife write some value as Master Offset value to Softmotion axis linked to master axis to get the next Sync point for the connected Slaves basis on the TouchProbe point and Cut to length point. If you are using common SoftMotion axis for both the slave as master then both the function block will write different Master offset value and create malfunctioning for both the Slave axis to get the next sync points.

Apart from above there is not any limitation in using the number of Application function blocks.

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings