Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to use Altistart 48 Soft Starter in Methane Gas environment.
Methane is a flammable gas which creates explosive atmosphere.
So, using any type of electrical equipment in such environment is restricted based on ATEX, Ex and other (local) norms describing and dedicated for Hazardous Area Classification for Flammable Gases and Vapors.
So, if ATS48 has to be used in explosive atmosphere, the only solution is to close it inside the special cabinet which is ATEX/Ex certified (means to isolate ATS from methane).

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings